Source Settings

Some of these settings are also available in the Instrument View. The Settings tables contain one row for each available output.

Basic Settings

Priority Mode Sets the output priority mode (Voltage, Current, Power or Resistance).
Settings Sets the output Voltage, Current, Power or Resistance level.
Limit Limits the selected parameter at the specified value.
Output Range Sets the output range, for power modules with multiple ranges.
Measurement Range Sets the measurement range, for power modules with multiple ranges.

Sensing and Coupling

Sensing Sets the output sense to 2-wire or 4-wire.
Coupling Enables or disables the output coupling or synchronization between multiple output channels
On Delay Time Enter the On Delays for all outputs that will participate in the output on delay sequence.
Off Delay Time Enter the Off Delays for all outputs that will participate in the output off delay sequence.

OVP and OCP Settings

OVP Enables Over Voltage Protection (OVP) with a corresponding voltage level. Depending on the PS model, you can also set a Delay Time.
OCP Enables Over Current Protection (OCP) with a corresponding level.
Depending on the PS model, you can also set a Delay Time and specify if the start of the delay is initiated by any transition into CC mode, or only at the end of a settings change.
Clear If a protection function is triggered, remove the condition that caused the protection fault, then click the output's Clear button to reset the protection.

See Also